SPRZ487E May   2022  – June 2024 AM620-Q1 , AM623 , AM625 , AM625-Q1 , AM625SIP

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2103
      5.      i2134
      6.      i2189
      7.      i2196
      8.      i2232
      9.      i2244
      10.      i2310
      11.      i2311
      12.      i2327
      13.      i2328
      14.      i2279
      15.      i2307
      16.      i2320
      17.      i2329
      18.      i2208
      19.      i2249
      20.      i2278
      21.      i2312
      22.      i2366
      23.      i2371
      24.      i2253
      25.      i2283
      26.      i2383
      27.      i2401
      28.      i2407
      29.      i2409
      30.      i2410
      31.      i2413
      32.      i2414
      33.      i2415
      34.      i2416
      35.      i2417
      36.      i2418
      37.      i2419
      38.      i2420
      39.      i2421
      40.      i2422
      41.      i2423
      42.      i2435
  4.   Trademarks
  5.   Revision History

Usage Notes and Advisories Matrices

Table 1-1 lists all usage notes and the applicable silicon revision(s). Table 1-2 lists all advisories, modules affected, and the applicable silicon revision(s).

Table 1-1 Usage Notes Matrix
ID DESCRIPTION SILICON REVISIONS AFFECTED
AM62x 1.0 , AM625SIP 1.0
Boot i2372 — ROM doesn't support select multi-plane addressing schemes in Serial NAND boot YES
OSPI i2351 — OSPI: Controller does not support Continuous Read mode with NAND Flash YES
Table 1-2 Advisories Matrix
MODULE DESCRIPTION SILICON REVISIONS AFFECTED
AM62x 1.0 , AM625SIP 1.0
Boot i2307 — Boot: ROM does not properly select OSPI clocking modes based on BOOTMODE YES
Boot i2328 — Boot: USB MSC boots intermittently YES
Boot i2366 — Boot: ROM does not comprehend specific JEDEC SFDP features for 8D-8D-8D operation YES
Boot i2371 — Boot: ROM code may hang in UART boot mode during data transfer YES
Boot i2410 — Boot: ROM may fail to boot due to i2409 YES
Boot i2413 — Boot: HS-FS ROM boots corrupted ROM boot image YES
Boot i2414 — Boot: Ethernet PHY Scan and Bring-Up Flow doesn't work with PHYs that don't support Auto Negotiation YES
Boot i2415 — Boot: UART Backup Boot Authentication Failure w/ xSPI Primary Boot Mode YES
Boot i2416 — Boot: FAT boot partition with ESP flag doesn't boot YES
Boot i2417 — Boot: GPMC NAND configured to slower clock speed YES
Boot i2418 — Boot: Secure ROM Panic due to Certificate Info not present YES
Boot i2419 — Boot: When disabling deskew calibration, ROM does not check if deskew calibration was enabled YES
Boot i2420 — Boot: XSPI Boot time is not consistent in SFDP mode YES
Boot i2421 — Boot: fatTiny GPT handling causes data abort YES
Boot i2422 — Boot: ROM timeout for MMCSD filesystem boot too long YES
Boot i2423 — Boot: HS-FS ROM applies debug access restrictions to all address space covered by the efuse controller firewall YES
Boot i2435 — Boot: ROM timeout for eMMC boot too long YES
CPSW i2208 — CPSW: ALE IET Express Packet Drops YES
CPSW i2401 — CPSW: Host Timestamps Cause CPSW Port to Lock up YES
DDR i2232 — DDR: Controller postpones more than allowed refreshes after frequency change YES
DDR i2244 — DDR: Valid stop value must be defined for write DQ VREF training YES
DEBUG i2283 — Restrictions on how CP Tracer Debug Probes can be used YES
DMA i2320 — BCDMA, PKTDMA: Descriptors and TRs required to be returned unfragmented YES
DSS i2097 — DSS: Disabling a layer connected to Overlay may result in synclost during the next frame YES
ECC_AGGR i2049 — ECC_AGGR: Potential IP Clockstop/Reset Sequence Hang due to Pending ECC Aggregator Interrupts YES
Internal Diagnostic Modules i2103 — Incorrect Reporting of ECC_GRP, ECC_BIT and ECC_TYPE Information for Functional Safety Errors YES
Interrupt Aggregator i2196 — IA: Potential deadlock scenarios in IA YES
MCAN i2279 — MCAN: Specification Update for dedicated Tx Buffers and Tx Queues configured with same Message ID YES
MCAN i2278 — MCAN: Message Transmit order not guaranteed from dedicated Tx Buffers configured with same Message ID YES
MDIO i2329 — MDIO: MDIO interface corruption (CPSW and PRU-ICSS) YES
MMCSD i2312 — MMCSD: HS200 and SDR104 Command Timeout Window Too Small YES
OSPI i2189 — OSPI: Controller PHY Tuning Algorithm YES
OSPI i2249 — OSPI: Internal PHY Loopback and Internal Pad Loopback clocking modes with DDR timing inoperable YES
OSPI i2383 — OSPI: 2-byte address is not supported in PHY DDR mode YES
PRG i2253 — PRG: CTRL_MMR STAT registers are unreliable indicators of POK threshold failure YES
RAT i2062 — RAT: Error Interrupt Triggered Even When Error Logging Disable Is Set YES
RESET i2407— RESET: MCU_RESETSTATz unreliable when MCU_RESETz is asserted low YES
RTC i2327 — RTC: Hardware wakeup event limitation YES
USART i2310 — USART: Erroneous clear/trigger of timeout interrupt YES
USART i2311 — USART Spurious DMA Interrupts YES
USB i2134 — USB: 2.0 Compliance Receive Sensitivity Test Limitation YES
USB i2409 — USB: USB2 PHY locks up due to short suspend YES