SPRZ544B March   2023  – December 2024 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2134
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2208
      9.      i2249
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2366
      16.      i2371
      17.      i2120
      18.      i2137
      19.      i2190
      20.      i2253
      21.      i2373
      22.      i2383
      23.      i2401
      24.      i2407
      25.      i2409
      26.      i2410
      27.      i2376
      28.      i2399
      29.      i2413
      30.      i2414
      31.      i2419
      32.      i2420
      33.      i2421
      34.      i2422
      35.      i2423
      36.      i2431
      37.      i2435
  4.   Trademarks
  5.   Revision History

i2310

USART: Erroneous clear/trigger of timeout interrupt

Details:

The USART may erroneously clear or trigger the timeout interrupt when RHR/MSR/LSR registers are read.

Workaround(s):

For CPU use-case.

  • If the timeout interrupt is erroneously cleared:
    • This is Valid since the pending data inside the FIFO will retrigger the timeout interrupt
  • If timeout interrupt is erroneously set, and the FIFO is empty, use the following SW workaround to clear the interrupt:
    • Set a high value of timeout counter in TIMEOUTH and TIMEOUTL registers
    • Set EFR2 bit 6 to 1 to change timeout mode to periodic
    • Read the IIR register to clear the interrupt
    • Set EFR2 bit 6 back to 0 to change timeout mode back to the original mode

For DMA use-case.

  • If timeout interrupt is erroneously cleared:
    • This is valid since the next periodic event will retrigger the timeout interrupt
    • User must ensure that RX timeout behavior is in periodic mode by setting EFR2 bit6 to 1
  • If timeout interrupt is erroneously set:
    • This will cause DMA to be torn down by the SW driver
    • Valid since next incoming data will cause SW to setup DMA again