SPRZ544B March   2023  – December 2024 AM62A1-Q1 , AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
      3.      i2424
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2097
      4.      i2134
      5.      i2189
      6.      i2196
      7.      i2199
      8.      i2208
      9.      i2249
      10.      i2278
      11.      i2279
      12.      i2310
      13.      i2311
      14.      i2312
      15.      i2366
      16.      i2371
      17.      i2120
      18.      i2137
      19.      i2190
      20.      i2253
      21.      i2373
      22.      i2383
      23.      i2401
      24.      i2407
      25.      i2409
      26.      i2410
      27.      i2376
      28.      i2399
      29.      i2413
      30.      i2414
      31.      i2419
      32.      i2420
      33.      i2421
      34.      i2422
      35.      i2423
      36.      i2431
      37.      i2435
  4.   Trademarks
  5.   Revision History

i2376

C7x: SE/SA/HWAOPEN receives corrupted template following two back to back VPUT/MVC instructions

Details

On the C7604 CPU, programming information is sent to the Streaming Engines via SEOPEN, the Streaming Address Generators via SAOPEN, and to the MMA via the HWAOPEN instructions. This programming information is sourced from CUCR registers in the CPU that are populated and updated via the MVC and VPUT family of instructions. Data being written into these CUCR registers can be incorrectly forwarded to the SEOPEN, SAOPEN, and HWAOPEN instructions if in a sequence of three CPU cycles a CUCR register is updated on the first two cycles and then used by an SEOPEN, SAOPEN, or HWAOPEN instruction on the third.

For example, this sequence will cause a forwarding error to occur in the execution of the SAOPEN instruction, corrupting SA0's programming:

MVC .C2 VB0, CUCR0
VPUTD .C2 B1, 0, CUCR0
SAOPEN .C2 CUCR1:CUCR0, 0

Workaround

The issue can be avoided by avoiding the sequence of three execute packets where the first two contain MVC/VPUT instructions that write to the same CUCR and the third contains an SE/SA/HWAOPEN instruction that reads from the same. The workaround is included automatically by the compiler when compiling C7504 code.