SPRZ580 December   2024 AM62D-Q1

 

  1.   1
  2. 1Usage Notes and Advisories Matrices
    1. 1.1 Devices Supported
  3. 2Silicon Usage Notes and Advisories
    1. 2.1 Silicon Usage Notes
      1.      i2351
      2.      i2372
    2. 2.2 Silicon Advisories
      1.      i2049
      2.      i2062
      3.      i2134
      4.      i2189
      5.      i2196
      6.      i2199
      7.      i2208
      8.      i2249
      9.      i2278
      10.      i2279
      11.      i2310
      12.      i2311
      13.      i2312
      14.      i2366
      15.      i2371
      16.      i2120
      17.      i2137
      18.      i2253
      19.      i2383
      20.      i2401
      21.      i2407
      22.      i2409
      23.      i2410
      24.      i2376
      25.      i2399
      26.      i2413
      27.      i2414
      28.      i2417
      29.      i2419
      30.      i2420
      31.      i2421
      32.      i2422
      33.      i2423
      34.      i2431
      35.      i2435
  4.   Trademarks
  5.   Revision History

i2435

Boot: ROM timeout for eMMC boot too long

Details:

Due to a bug in ROM, if attempting to boot in eMMC boot mode (ie, from eMMC boot partitions, sometimes referred to as eMMC alternative mode) from an eMMC device that is empty or erased (or factory fresh), the normal boot timeout to switch to backup boot mode will take 10 seconds.

Workaround(s):

Need to boot from another boot mode if this timeout considered too long in the system.