Powering industrial Ethernet devices requires addressing specific aspects of industrial Ethernet and industrial applications.
The biggest difference between standard Ethernet and industrial Ethernet is the topology, as shown in Figure 1. Standard Ethernet is a star topology, whereas industrial Ethernet includes a variety of line, tree and ring topologies.
Aside from the topology, factory automation devices operate at 24V, whereas telecom devices are powered at 48V. While those different versions have existed for a long time, the first power solution for Industrial Ethernet was just released: EtherCAT P. In this blog post, I’ll explain what EtherCAT P is before covering alternatives for 1000BASE-T and/or ring topologies or single twisted pair.
As more factories worldwide use Ethernet to connect, there is a growing need to optimize the power distribution to the edge of the processes. A natural option would be to reuse the power over Ethernet (PoE) technology to power Ethernet-connected devices. The benefit of PoE technology is that it uses the same wires for power and data transfer, which saves on both the installation and total wiring costs, as shown in the factory automation system example shown in Figure 2. For this, the PoE power couples into the data lines by connecting 48V to the center tap of the Ethernet transformer of one pair and the return path similarly with another pair. Power then decouples at the slave device with a similar topology.
However, in the case of an industrial Ethernet with a line topology, the 25MHz of the Ethernet communication will be available at the output of the power supply and could therefore be coupled out on the transmit side. In that case, the transmitter would then suffer from noise from the receiver channel communication standard.
For this reason, EtherCAT P (which is an extension to EtherCAT) introduces a simple inductor-capacitor (LC) filter to ensure that the 25MHz from the 100BASE-T will be blocked before entering the power tree.
Another difference between PoE and EtherCAT P is that PoE offers only one 48V supply voltage, while EtherCAT P provides two independent 24V rails that are isolated from each other, shown in Table 1. In terms of power, PoE can deliver 71W (for 803.2bt Type 4), while EtherCAT P offers 24V x 3A ≥72W per voltage rail.
A major difference between the two technologies is that for PoE, you need two semiconductors for identification between the power-sourcing equipment (PSE) and the powered device (PD). The chip inside the PD is also responsible for setting the maximum power limit. But this brings two advantages: full power is only available if a valid connection is established, and PoE-capable devices can connect to non-PoE devices without damaging them.
In the case of EtherCAT P, you only need standard passives to couple power in – no additional semiconductors. This means the 24V supply is always present on the data line. However, the maximum power must be limited inside the PSE.
POE | EtherCAT P | |
---|---|---|
Supply voltage | 48V | 2 x 24V (Us and Up, isolated form each other) |
Power available at PD | Up to 71W for 803.3bt Type 4 | 2 x 72W (2 x 24V, 3A) |
Identification before Power | Yes | No |
Topologies | Point to point | Star, line, tree |
The EtherCAT P One Cable for Power and EtherCAT Reference Design shows an implementation of the power couple in-couple out circuitry of an EtherCAT P PSE. The reference design meets all requirements from the official “EtherCAT and EtherCAT P Slave Implementation Guide.” These requirements include features like reverse polarity protection, in-rush current limit and continuous current limit, all based on semiconductors from TI.
For EtherCAT communication, the reference design can connect to an EtherCAT-capable communication platform like the AMIC110 industrial communication engine (ICE) with an Ethernet cable. To showcase the power transfer functionality, you can connect two design boards with an EtherCAT P cable. You can also connect an EtherCAT master to the first reference design and an EtherCAT slave to the second reference design for a complete EtherCAT P demonstration system. For additional ease of evaluation, an optional 5V/12V buck module can be mounted onto the board as well.
Should your designs require compliance with Institute of Electrical and Electronics Engineers (IEEE) 802.3, check out the IEEE802.3bt New Features video, which will introduce you to the new IEEE 802.3bt PoE standard.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated