Deric Waters
Updated 4/16/2021: With the USB Implementers Forum (IF) standards body no longer certifying USB Power Delivery (PD) 2.0 silicon and end products, the time has come to move from USB PD 2.0 to USB PD 3.0. USB-IF certification provides products with the right to license the USB-IF Logo and ensures compliance with other USB certified end products and cables. Although Texas Instruments does not plan to end of life PD 2.0 devices, there is no longer a path to compliance using PD 2.0 silicon. USB PD 3.0’s expanded feature set and messaging have made it crucial to creating systems with USB PD. Let’s take a closer look at which features are specific to USB PD 3.0.
The main feature difference between USB PD 3.0 and USB PD 2.0 is the wide variety of optional messages that enable the source and sink to exchange more detailed and useful information. The required changes in USB PD 3.0 update the system to handle the larger number of these optional messages. These new messages do not interfere with negotiation and backward compatibility, and a USB PD 3.0 device is capable of negotiating with a USB PD 2.0 device. The source and sink message collision avoidance and the Not_Supported control message are two required changes that create a robust system which can work with these optional messages. The complete list of messages and changes can be seen below in Table 1.
Another new feature that comes with USB PD 3.0 is the Fast Role Swap (FRS) mechanism. With many systems needing the flexibility to be a Dual Role Port (DRP), there also comes the need to be able to switch between sourcing and sinking power fast enough that any USB data does not become corrupted nor video interrupted. FRS enables this quick change and protects the USB data in the process.
Table 1 lists the differences between the two versions as listed in the USB PD 3.0 specification.
![]() |
Let’s dispel the erroneous thought that the voltage profiles or power rules are different between USB PD 2.0 and USB PD 3.0. The power rules are identical in both PD versions. The most important rules are:
USB PD 3.0 ensures backwards compatibility with USB PD 2.0. All USB PD 3.0 sources and sinks are required to fully interoperate with USB PD 2.0 sources and sinks. This requirement is enforced by requiring all USB PD 3.0 devices to pass USB PD 2.0 compliance tests. From the USB-IF point of view, there are only USB PD products. The USB-IF does not distinguish between USB PD 2.0 products and USB PD 3.0 products when issuing USB logo certification.
TI offers many USB PD 3.0 compliant parts. Additionally, you can reach out to a device expert any time to help transition your system from USB PD 2.0 to 3.0 on our E2E forum.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated