Zachary Stokes
At some point while working with electronics, you have inevitably smelled the unmistakable scent of burning silicon. That’s what reverse current can do to your system. Reverse current is an event in which current travels in the opposite direction it should be moving through a system due to a high reverse bias voltage; from output to input. Fortunately, there are a handful of ways to protect your system from reverse current. This is the first blog of a series about reverse current protection, and will give a high-level overview of the solutions that exist.
The most common cause of reverse current, reverse bias voltage, is having a higher voltage on your output than on your input, inducing current to travel through your system in the opposite direction from what you intended. This can be seen in Figure 1.
This can happen because suddenly VIN becomes zero due to a power loss, leaving a higher voltage on the systems output than the input. Or perhaps power MUXing has accidentally caused a reverse voltage event.
Reverse current can potentially damage both internal circuitry and power supplies such as batteries. In fact, even cables can be damaged, and connectors degraded. This is why things burn up, because the large currents lead to an exponential rise in power dissipation.
Protection necessitates keeping reverse current flow very low. This means limiting reverse voltage. There are three common ways to protect from reverse current: designing a system using diodes, FETs, or load switches.
Between diodes and FETs, diodes cost less and are simpler to integrate. They are great for high-voltage, low-current applications. However, if you’ve ever used a diode, you’re surely familiar with the forward voltage drop that it causes, which shortens battery life and limits VCC by (generally) around 0.6-0.8 V. This voltage drop can lower the efficiency of the power circuitry, and increase the total power dissipation in the system.
For these reasons, a Schottky diode is a popular alternative; they have lower forward voltage drops. But they’re also more expensive and have higher reverse current leakage, which could cause problems for a system. Figure 2 shows a diode used in a system to block reverse current.
FETs are useful due to their low forward voltage drop and high current-handling capabilities, which are helpful when you must maintain lower power dissipation. For an N-type metal-oxide-semiconductor (NMOS) FET set in the ground path, you orient the body diode in the direction of normal current flow. That way, if someone installs the battery incorrectly, the gate voltage is low, which prevents the FET from turning on. When the battery is installed correctly, however, the gate voltage is high and its channel shorts out to ground.
You can also put FETs back to back in order to block current in both directions when the FETs are turned off. Compared to the diode solution, there is a lower voltage drop from the power supply to the load, but this implementation takes up a larger amount of board real estate. Figure 3 shows an example of back to back FETs used for blocking reverse current.
TI load switches are integrated electronic relays used to turn power rails on and off. Most basic load switches consist of four pins: input voltage, output voltage, enable, and ground, and include a multitude of features, including reverse current protection, in a small, integrated package. Figure 4 shows a load switch used to block reverse current.
For example, Texas Instruments’ TPS22963 3A load switch integrates reverse current protection and more, all in a 1.4mm x .9mm package. Figure 5 shows typical placement for the TPS22963 in a system.
Reverse current can be caused for a few reasons, whether it be a sudden loss of VIN or an accident in power MUXing. This can result in system damage or even power-supply damage. TI load switches can be a size-efficient, cost-effective solution for managing reverse current.
Learn more about TI’s load switch solutions with reverse current protection.
Read the blog: What is a load switch?
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2023, Texas Instruments Incorporated