SWCU191 February 2022 CC1311P3 , CC1311R3 , CC2651P3 , CC2651R3 , CC2651R3SIPA
#CPU_TPIU_CPU_TPIU_MAP1_TABLE_1 lists the memory-mapped registers for the CPU_TPIU registers. All register offset addresses not listed in #CPU_TPIU_CPU_TPIU_MAP1_TABLE_1 should be considered as reserved locations and the register contents should not be modified.
Offset | Acronym | Register Name | Section |
---|---|---|---|
0h | SSPSR | Supported Sync Port Sizes | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_SSPSR |
4h | CSPSR | Current Sync Port Size | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CSPSR |
10h | ACPR | Async Clock Prescaler | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_ACPR |
F0h | SPPR | Selected Pin Protocol | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_SPPR |
300h | FFSR | Formatter and Flush Status | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FFSR |
304h | FFCR | Formatter and Flush Control | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FFCR |
308h | FSCR | Formatter Synchronization Counter | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FSCR |
FA0h | CLAIMMASK | Claim Tag Mask | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMMASK |
FA0h | CLAIMSET | Claim Tag Set | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMSET |
FA4h | CLAIMTAG | Current Claim Tag | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMTAG |
FA4h | CLAIMCLR | Claim Tag Clear | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMCLR |
FC8h | DEVID | Device ID | #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_DEVID |
Complex bit access types are encoded to fit into small table cells. #CPU_TPIU_CPU_TPIU_MAP1_LEGEND shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Write Type | ||
W | W | Write |
Reset or Default Value | ||
-n | Value after reset or the default value |
SSPSR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_SSPSR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_SSPSR_TABLE.
Return to the Summary Table.
Supported Sync Port Sizes
This register represents a single port size that is supported on the device, that is, 4, 2 or 1. This is to ensure that tools do not attempt to select a port width that an attached TPA cannot capture.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | FOUR | THREE | TWO | ONE | |||
R-0h | R-1h | R-0h | R-1h | R-1h | |||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-4 | RESERVED | R | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
3 | FOUR | R | 1h | 4-bit port size support 0x0: Not supported 0x1: Supported |
2 | THREE | R | 0h | 3-bit port size support 0x0: Not supported 0x1: Supported |
1 | TWO | R | 1h | 2-bit port size support 0x0: Not supported 0x1: Supported |
0 | ONE | R | 1h | 1-bit port size support 0x0: Not supported 0x1: Supported |
CSPSR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CSPSR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CSPSR_TABLE.
Return to the Summary Table.
Current Sync Port Size
This register has the same format as SSPSR but only one bit can be set, and all others must be zero. Writing values with more than one bit set, or setting a bit that is not indicated as supported can cause Unpredictable behavior. On reset this defaults to the smallest possible port size, 1 bit.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R/W-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R/W-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | FOUR | THREE | TWO | ONE | |||
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-1h | |||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-4 | RESERVED | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
3 | FOUR | R/W | 0h | 4-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
2 | THREE | R/W | 0h | 3-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
1 | TWO | R/W | 0h | 2-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
0 | ONE | R/W | 1h | 1-bit port enable Writing values with more than one bit set in CSPSR, or setting a bit that is not indicated as supported in SSPSR can cause Unpredictable behavior. |
ACPR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_ACPR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_ACPR_TABLE.
Return to the Summary Table.
Async Clock Prescaler
This register scales the baud rate of the asynchronous output.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PRESCALER | ||||||||||||||||||||||||||||||
R/W-0h | R/W-0h | ||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-13 | RESERVED | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
12-0 | PRESCALER | R/W | 0h | Divisor for input trace clock is (PRESCALER + 1). |
SPPR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_SPPR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_SPPR_TABLE.
Return to the Summary Table.
Selected Pin Protocol
This register selects the protocol to be used for trace output.
Note: If this register is changed while trace data is being output, data corruption occurs.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R/W-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R/W-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R/W-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | PROTOCOL | ||||||
R/W-0h | R/W-1h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-2 | RESERVED | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
1-0 | PROTOCOL | R/W | 1h | Trace output protocol
0h = TracePort mode 1h = SerialWire Output (Manchester). This is the reset value. 2h = SerialWire Output (NRZ) |
FFSR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FFSR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FFSR_TABLE.
Return to the Summary Table.
Formatter and Flush Status
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | |||||||
R-0h | |||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | FTNONSTOP | RESERVED | |||||
R-0h | R-1h | R-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-4 | RESERVED | R | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
3 | FTNONSTOP | R | 1h | 0: Formatter can be stopped 1: Formatter cannot be stopped |
2-0 | RESERVED | R | 0h | This field always reads as zero |
FFCR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FFCR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FFCR_TABLE.
Return to the Summary Table.
Formatter and Flush Control
When one of the two single wire output (SWO) modes is selected, ENFCONT enables the formatter to be bypassed. If the formatter is bypassed, only the ITM/DWT trace source (ATDATA2) passes through. The TPIU accepts and discards data that is presented on the ETM port (ATDATA1). This function is intended to be used when it is necessary to connect a device containing an ETM to a trace capture device that is only able to capture Serial Wire Output (SWO) data. Enabling or disabling the formatter causes momentary data corruption.
Note: If the selected pin protocol register (SPPR.PROTOCOL) is set to 0x00 (TracePort mode), this register always reads 0x102, because the formatter is automatically enabled. If one of the serial wire modes is then selected, the register reverts to its previously programmed value.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | |||||||
R/W-0h | |||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | |||||||
R/W-0h | |||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | TRIGIN | ||||||
R/W-0h | R/W-1h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | ENFCONT | RESERVED | |||||
R/W-0h | R/W-1h | R/W-0h | |||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-9 | RESERVED | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
8 | TRIGIN | R/W | 1h | Indicates that triggers are inserted when a trigger pin is asserted. |
7-2 | RESERVED | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
1 | ENFCONT | R/W | 1h | Enable continuous formatting: 0: Continuous formatting disabled 1: Continuous formatting enabled |
0 | RESERVED | R/W | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
FSCR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FSCR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_FSCR_TABLE.
Return to the Summary Table.
Formatter Synchronization Counter
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
FSCR | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | FSCR | R | 0h | The global synchronization trigger is generated by the Program Counter (PC) Sampler block. This means that there is no synchronization counter in the TPIU. |
CLAIMMASK is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMMASK_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMMASK_TABLE.
Return to the Summary Table.
Claim Tag Mask
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CLAIMMASK | |||||||||||||||||||||||||||||||
R-Fh | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | CLAIMMASK | R | Fh | This register forms one half of the Claim Tag value. When reading this register returns the number of bits that can be set (each bit is considered separately): 0: This claim tag bit is not implemented 1: This claim tag bit is not implemented The behavior when writing to this register is described in CLAIMSET. |
CLAIMSET is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMSET_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMSET_TABLE.
Return to the Summary Table.
Claim Tag Set
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CLAIMSET | |||||||||||||||||||||||||||||||
W-Fh | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | CLAIMSET | W | Fh | This register forms one half of the Claim Tag value. Writing to this location allows individual bits to be set (each bit is considered separately): 0: No effect 1: Set this bit in the claim tag The behavior when reading from this location is described in CLAIMMASK. |
CLAIMTAG is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMTAG_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMTAG_TABLE.
Return to the Summary Table.
Current Claim Tag
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CLAIMTAG | |||||||||||||||||||||||||||||||
R-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | CLAIMTAG | R | 0h | This register forms one half of the Claim Tag value. Reading this register returns the current Claim Tag value. Reading CLAIMMASK determines how many bits from this register must be used. The behavior when writing to this register is described in CLAIMCLR. |
CLAIMCLR is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMCLR_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_CLAIMCLR_TABLE.
Return to the Summary Table.
Claim Tag Clear
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
CLAIMCLR | |||||||||||||||||||||||||||||||
W-0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | CLAIMCLR | W | 0h | This register forms one half of the Claim Tag value. Writing to this location enables individual bits to be cleared (each bit is considered separately): 0: No effect 1: Clear this bit in the claim tag. The behavior when reading from this location is described in CLAIMTAG. |
DEVID is shown in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_DEVID_FIGURE and described in #CPU_TPIU_CPU_TPIU_MAP1_CPU_TPIU_ALL_DEVID_TABLE.
Return to the Summary Table.
Device ID
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DEVID | |||||||||||||||||||||||||||||||
R-CA0h | |||||||||||||||||||||||||||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-0 | DEVID | R | CA0h | This field returns: 0xCA1 if there is an ETM present. 0xCA0 if there is no ETM present. |