SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
The cache contains a TAG prefetch system that automatically prefetches the TAG data for the next 64-bit address. This feature is controlled through the VIMS:CTL.PREF_EN register, and is only enabled if the VIMS mode is set to cache mode. Any access using a prefetched TAG saves one CLK cycle in the access because tag lookup can be skipped. A prefetch hit is defined as an access using prefetched TAG data and data that is available in the cache.
TAG prefetch is mainly intended for performance optimization when the CPU is running at full speed. If the CPU is not running at full speed, there is no performance optimization; therefore the TAG prefetch system should be disabled to minimize power consumption.