SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
The procedure takes the following input parameter:
The procedure returns the following:
The procedure returns with error if the specified queue is empty. Otherwise, the following is done:
Set pQueue->pCurrEntry->status = Active