SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
#MCU_GPIO_MCU_GPIO_MAP1_TABLE_1 lists the memory-mapped registers for the MCU_GPIO registers. All register offset addresses not listed in #MCU_GPIO_MCU_GPIO_MAP1_TABLE_1 should be considered as reserved locations and the register contents should not be modified.
Complex bit access types are encoded to fit into small table cells. #MCU_GPIO_MCU_GPIO_MAP1_LEGEND shows the codes that are used for access types in this section.
Access Type | Code | Description |
---|---|---|
Read Type | ||
R | R | Read |
Write Type | ||
W | W | Write |
W1C | W 1C | Write 1 to clear |
W1S | W 1S | Write 1 to set |
Reset or Default Value | ||
-n | Value after reset or the default value |
DOUT3_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT3_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT3_0_TABLE.
Return to the Summary Table.
Data Out 0 to 3
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO3 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO2 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO1 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO0 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO3 | W | 0h | Sets the state of the pin that is configured as DIO#3, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO2 | W | 0h | Sets the state of the pin that is configured as DIO#2, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO1 | W | 0h | Sets the state of the pin that is configured as DIO#1, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO0 | W | 0h | Sets the state of the pin that is configured as DIO#0, if the corresponding DOE31_0 bitfield is set. |
DOUT7_4 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT7_4_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT7_4_TABLE.
Return to the Summary Table.
Data Out 4 to 7
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO7 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO6 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO5 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO4 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO7 | W | 0h | Sets the state of the pin that is configured as DIO#7, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO6 | W | 0h | Sets the state of the pin that is configured as DIO#6, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO5 | W | 0h | Sets the state of the pin that is configured as DIO#5, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO4 | W | 0h | Sets the state of the pin that is configured as DIO#4, if the corresponding DOE31_0 bitfield is set. |
DOUT11_8 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT11_8_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT11_8_TABLE.
Return to the Summary Table.
Data Out 8 to 11
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO11 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO10 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO9 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO8 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO11 | W | 0h | Sets the state of the pin that is configured as DIO#11, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO10 | W | 0h | Sets the state of the pin that is configured as DIO#10, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO9 | W | 0h | Sets the state of the pin that is configured as DIO#9, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO8 | W | 0h | Sets the state of the pin that is configured as DIO#8, if the corresponding DOE31_0 bitfield is set. |
DOUT15_12 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT15_12_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT15_12_TABLE.
Return to the Summary Table.
Data Out 12 to 15
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO15 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO14 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO13 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO12 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO15 | W | 0h | Sets the state of the pin that is configured as DIO#15, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO14 | W | 0h | Sets the state of the pin that is configured as DIO#14, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO13 | W | 0h | Sets the state of the pin that is configured as DIO#13, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO12 | W | 0h | Sets the state of the pin that is configured as DIO#12, if the corresponding DOE31_0 bitfield is set. |
DOUT19_16 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT19_16_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT19_16_TABLE.
Return to the Summary Table.
Data Out 16 to 19
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO19 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO18 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO17 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO16 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO19 | W | 0h | Sets the state of the pin that is configured as DIO#19, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO18 | W | 0h | Sets the state of the pin that is configured as DIO#18, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO17 | W | 0h | Sets the state of the pin that is configured as DIO#17, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO16 | W | 0h | Sets the state of the pin that is configured as DIO#16, if the corresponding DOE31_0 bitfield is set. |
DOUT23_20 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT23_20_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT23_20_TABLE.
Return to the Summary Table.
Data Out 20 to 23
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO23 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO22 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO21 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO20 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO23 | W | 0h | Sets the state of the pin that is configured as DIO#23, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO22 | W | 0h | Sets the state of the pin that is configured as DIO#22, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO21 | W | 0h | Sets the state of the pin that is configured as DIO#21, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO20 | W | 0h | Sets the state of the pin that is configured as DIO#20, if the corresponding DOE31_0 bitfield is set. |
DOUT27_24 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT27_24_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT27_24_TABLE.
Return to the Summary Table.
Data Out 24 to 27
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO27 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO26 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO25 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO24 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO27 | W | 0h | Sets the state of the pin that is configured as DIO#27, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO26 | W | 0h | Sets the state of the pin that is configured as DIO#26, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO25 | W | 0h | Sets the state of the pin that is configured as DIO#25, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO24 | W | 0h | Sets the state of the pin that is configured as DIO#24, if the corresponding DOE31_0 bitfield is set. |
DOUT31_28 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT31_28_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT31_28_TABLE.
Return to the Summary Table.
Data Out 28 to 31
Alias register for byte access to each bit in DOUT31_0
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
RESERVED | DIO31 | ||||||
R-0h | W-0h | ||||||
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
RESERVED | DIO30 | ||||||
R-0h | W-0h | ||||||
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
RESERVED | DIO29 | ||||||
R-0h | W-0h | ||||||
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RESERVED | DIO28 | ||||||
R-0h | W-0h | ||||||
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31-25 | RESERVED | R | 0h | Reserved |
24 | DIO31 | W | 0h | Sets the state of the pin that is configured as DIO#31, if the corresponding DOE31_0 bitfield is set. |
23-17 | RESERVED | R | 0h | Reserved |
16 | DIO30 | W | 0h | Sets the state of the pin that is configured as DIO#30, if the corresponding DOE31_0 bitfield is set. |
15-9 | RESERVED | R | 0h | Reserved |
8 | DIO29 | W | 0h | Sets the state of the pin that is configured as DIO#29, if the corresponding DOE31_0 bitfield is set. |
7-1 | RESERVED | R | 0h | Reserved |
0 | DIO28 | W | 0h | Sets the state of the pin that is configured as DIO#28, if the corresponding DOE31_0 bitfield is set. |
DOUT31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUT31_0_TABLE.
Return to the Summary Table.
Data Output for DIO 0 to 31
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | R/W | 0h | Data output for DIO 31 |
30 | DIO30 | R/W | 0h | Data output for DIO 30 |
29 | DIO29 | R/W | 0h | Data output for DIO 29 |
28 | DIO28 | R/W | 0h | Data output for DIO 28 |
27 | DIO27 | R/W | 0h | Data output for DIO 27 |
26 | DIO26 | R/W | 0h | Data output for DIO 26 |
25 | DIO25 | R/W | 0h | Data output for DIO 25 |
24 | DIO24 | R/W | 0h | Data output for DIO 24 |
23 | DIO23 | R/W | 0h | Data output for DIO 23 |
22 | DIO22 | R/W | 0h | Data output for DIO 22 |
21 | DIO21 | R/W | 0h | Data output for DIO 21 |
20 | DIO20 | R/W | 0h | Data output for DIO 20 |
19 | DIO19 | R/W | 0h | Data output for DIO 19 |
18 | DIO18 | R/W | 0h | Data output for DIO 18 |
17 | DIO17 | R/W | 0h | Data output for DIO 17 |
16 | DIO16 | R/W | 0h | Data output for DIO 16 |
15 | DIO15 | R/W | 0h | Data output for DIO 15 |
14 | DIO14 | R/W | 0h | Data output for DIO 14 |
13 | DIO13 | R/W | 0h | Data output for DIO 13 |
12 | DIO12 | R/W | 0h | Data output for DIO 12 |
11 | DIO11 | R/W | 0h | Data output for DIO 11 |
10 | DIO10 | R/W | 0h | Data output for DIO 10 |
9 | DIO9 | R/W | 0h | Data output for DIO 9 |
8 | DIO8 | R/W | 0h | Data output for DIO 8 |
7 | DIO7 | R/W | 0h | Data output for DIO 7 |
6 | DIO6 | R/W | 0h | Data output for DIO 6 |
5 | DIO5 | R/W | 0h | Data output for DIO 5 |
4 | DIO4 | R/W | 0h | Data output for DIO 4 |
3 | DIO3 | R/W | 0h | Data output for DIO 3 |
2 | DIO2 | R/W | 0h | Data output for DIO 2 |
1 | DIO1 | R/W | 0h | Data output for DIO 1 |
0 | DIO0 | R/W | 0h | Data output for DIO 0 |
DOUTSET31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUTSET31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUTSET31_0_TABLE.
Return to the Summary Table.
Data Out Set
Writing 1 to a bit position sets the corresponding bit in the DOUT31_0 register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h | W1S-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | W1S | 0h | Set bit 31 |
30 | DIO30 | W1S | 0h | Set bit 30 |
29 | DIO29 | W1S | 0h | Set bit 29 |
28 | DIO28 | W1S | 0h | Set bit 28 |
27 | DIO27 | W1S | 0h | Set bit 27 |
26 | DIO26 | W1S | 0h | Set bit 26 |
25 | DIO25 | W1S | 0h | Set bit 25 |
24 | DIO24 | W1S | 0h | Set bit 24 |
23 | DIO23 | W1S | 0h | Set bit 23 |
22 | DIO22 | W1S | 0h | Set bit 22 |
21 | DIO21 | W1S | 0h | Set bit 21 |
20 | DIO20 | W1S | 0h | Set bit 20 |
19 | DIO19 | W1S | 0h | Set bit 19 |
18 | DIO18 | W1S | 0h | Set bit 18 |
17 | DIO17 | W1S | 0h | Set bit 17 |
16 | DIO16 | W1S | 0h | Set bit 16 |
15 | DIO15 | W1S | 0h | Set bit 15 |
14 | DIO14 | W1S | 0h | Set bit 14 |
13 | DIO13 | W1S | 0h | Set bit 13 |
12 | DIO12 | W1S | 0h | Set bit 12 |
11 | DIO11 | W1S | 0h | Set bit 11 |
10 | DIO10 | W1S | 0h | Set bit 10 |
9 | DIO9 | W1S | 0h | Set bit 9 |
8 | DIO8 | W1S | 0h | Set bit 8 |
7 | DIO7 | W1S | 0h | Set bit 7 |
6 | DIO6 | W1S | 0h | Set bit 6 |
5 | DIO5 | W1S | 0h | Set bit 5 |
4 | DIO4 | W1S | 0h | Set bit 4 |
3 | DIO3 | W1S | 0h | Set bit 3 |
2 | DIO2 | W1S | 0h | Set bit 2 |
1 | DIO1 | W1S | 0h | Set bit 1 |
0 | DIO0 | W1S | 0h | Set bit 0 |
DOUTCLR31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUTCLR31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUTCLR31_0_TABLE.
Return to the Summary Table.
Data Out Clear
Writing 1 to a bit position clears the corresponding bit in the DOUT31_0 register
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h | W1C-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | W1C | 0h | Clears bit 31 |
30 | DIO30 | W1C | 0h | Clears bit 30 |
29 | DIO29 | W1C | 0h | Clears bit 29 |
28 | DIO28 | W1C | 0h | Clears bit 28 |
27 | DIO27 | W1C | 0h | Clears bit 27 |
26 | DIO26 | W1C | 0h | Clears bit 26 |
25 | DIO25 | W1C | 0h | Clears bit 25 |
24 | DIO24 | W1C | 0h | Clears bit 24 |
23 | DIO23 | W1C | 0h | Clears bit 23 |
22 | DIO22 | W1C | 0h | Clears bit 22 |
21 | DIO21 | W1C | 0h | Clears bit 21 |
20 | DIO20 | W1C | 0h | Clears bit 20 |
19 | DIO19 | W1C | 0h | Clears bit 19 |
18 | DIO18 | W1C | 0h | Clears bit 18 |
17 | DIO17 | W1C | 0h | Clears bit 17 |
16 | DIO16 | W1C | 0h | Clears bit 16 |
15 | DIO15 | W1C | 0h | Clears bit 15 |
14 | DIO14 | W1C | 0h | Clears bit 14 |
13 | DIO13 | W1C | 0h | Clears bit 13 |
12 | DIO12 | W1C | 0h | Clears bit 12 |
11 | DIO11 | W1C | 0h | Clears bit 11 |
10 | DIO10 | W1C | 0h | Clears bit 10 |
9 | DIO9 | W1C | 0h | Clears bit 9 |
8 | DIO8 | W1C | 0h | Clears bit 8 |
7 | DIO7 | W1C | 0h | Clears bit 7 |
6 | DIO6 | W1C | 0h | Clears bit 6 |
5 | DIO5 | W1C | 0h | Clears bit 5 |
4 | DIO4 | W1C | 0h | Clears bit 4 |
3 | DIO3 | W1C | 0h | Clears bit 3 |
2 | DIO2 | W1C | 0h | Clears bit 2 |
1 | DIO1 | W1C | 0h | Clears bit 1 |
0 | DIO0 | W1C | 0h | Clears bit 0 |
DOUTTGL31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUTTGL31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOUTTGL31_0_TABLE.
Return to the Summary Table.
Data Out Toggle
Writing 1 to a bit position will invert the corresponding DIO output.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | R/W | 0h | Toggles bit 31 |
30 | DIO30 | R/W | 0h | Toggles bit 30 |
29 | DIO29 | R/W | 0h | Toggles bit 29 |
28 | DIO28 | R/W | 0h | Toggles bit 28 |
27 | DIO27 | R/W | 0h | Toggles bit 27 |
26 | DIO26 | R/W | 0h | Toggles bit 26 |
25 | DIO25 | R/W | 0h | Toggles bit 25 |
24 | DIO24 | R/W | 0h | Toggles bit 24 |
23 | DIO23 | R/W | 0h | Toggles bit 23 |
22 | DIO22 | R/W | 0h | Toggles bit 22 |
21 | DIO21 | R/W | 0h | Toggles bit 21 |
20 | DIO20 | R/W | 0h | Toggles bit 20 |
19 | DIO19 | R/W | 0h | Toggles bit 19 |
18 | DIO18 | R/W | 0h | Toggles bit 18 |
17 | DIO17 | R/W | 0h | Toggles bit 17 |
16 | DIO16 | R/W | 0h | Toggles bit 16 |
15 | DIO15 | R/W | 0h | Toggles bit 15 |
14 | DIO14 | R/W | 0h | Toggles bit 14 |
13 | DIO13 | R/W | 0h | Toggles bit 13 |
12 | DIO12 | R/W | 0h | Toggles bit 12 |
11 | DIO11 | R/W | 0h | Toggles bit 11 |
10 | DIO10 | R/W | 0h | Toggles bit 10 |
9 | DIO9 | R/W | 0h | Toggles bit 9 |
8 | DIO8 | R/W | 0h | Toggles bit 8 |
7 | DIO7 | R/W | 0h | Toggles bit 7 |
6 | DIO6 | R/W | 0h | Toggles bit 6 |
5 | DIO5 | R/W | 0h | Toggles bit 5 |
4 | DIO4 | R/W | 0h | Toggles bit 4 |
3 | DIO3 | R/W | 0h | Toggles bit 3 |
2 | DIO2 | R/W | 0h | Toggles bit 2 |
1 | DIO1 | R/W | 0h | Toggles bit 1 |
0 | DIO0 | R/W | 0h | Toggles bit 0 |
DIN31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DIN31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DIN31_0_TABLE.
Return to the Summary Table.
Data Input from DIO 0 to 31
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | R | 0h | Data input from DIO 31 |
30 | DIO30 | R | 0h | Data input from DIO 30 |
29 | DIO29 | R | 0h | Data input from DIO 29 |
28 | DIO28 | R | 0h | Data input from DIO 28 |
27 | DIO27 | R | 0h | Data input from DIO 27 |
26 | DIO26 | R | 0h | Data input from DIO 26 |
25 | DIO25 | R | 0h | Data input from DIO 25 |
24 | DIO24 | R | 0h | Data input from DIO 24 |
23 | DIO23 | R | 0h | Data input from DIO 23 |
22 | DIO22 | R | 0h | Data input from DIO 22 |
21 | DIO21 | R | 0h | Data input from DIO 21 |
20 | DIO20 | R | 0h | Data input from DIO 20 |
19 | DIO19 | R | 0h | Data input from DIO 19 |
18 | DIO18 | R | 0h | Data input from DIO 18 |
17 | DIO17 | R | 0h | Data input from DIO 17 |
16 | DIO16 | R | 0h | Data input from DIO 16 |
15 | DIO15 | R | 0h | Data input from DIO 15 |
14 | DIO14 | R | 0h | Data input from DIO 14 |
13 | DIO13 | R | 0h | Data input from DIO 13 |
12 | DIO12 | R | 0h | Data input from DIO 12 |
11 | DIO11 | R | 0h | Data input from DIO 11 |
10 | DIO10 | R | 0h | Data input from DIO 10 |
9 | DIO9 | R | 0h | Data input from DIO 9 |
8 | DIO8 | R | 0h | Data input from DIO 8 |
7 | DIO7 | R | 0h | Data input from DIO 7 |
6 | DIO6 | R | 0h | Data input from DIO 6 |
5 | DIO5 | R | 0h | Data input from DIO 5 |
4 | DIO4 | R | 0h | Data input from DIO 4 |
3 | DIO3 | R | 0h | Data input from DIO 3 |
2 | DIO2 | R | 0h | Data input from DIO 2 |
1 | DIO1 | R | 0h | Data input from DIO 1 |
0 | DIO0 | R | 0h | Data input from DIO 0 |
DOE31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOE31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_DOE31_0_TABLE.
Return to the Summary Table.
Data Output Enable for DIO 0 to 31
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | R/W | 0h | Data output enable for DIO 31 |
30 | DIO30 | R/W | 0h | Data output enable for DIO 30 |
29 | DIO29 | R/W | 0h | Data output enable for DIO 29 |
28 | DIO28 | R/W | 0h | Data output enable for DIO 28 |
27 | DIO27 | R/W | 0h | Data output enable for DIO 27 |
26 | DIO26 | R/W | 0h | Data output enable for DIO 26 |
25 | DIO25 | R/W | 0h | Data output enable for DIO 25 |
24 | DIO24 | R/W | 0h | Data output enable for DIO 24 |
23 | DIO23 | R/W | 0h | Data output enable for DIO 23 |
22 | DIO22 | R/W | 0h | Data output enable for DIO 22 |
21 | DIO21 | R/W | 0h | Data output enable for DIO 21 |
20 | DIO20 | R/W | 0h | Data output enable for DIO 20 |
19 | DIO19 | R/W | 0h | Data output enable for DIO 19 |
18 | DIO18 | R/W | 0h | Data output enable for DIO 18 |
17 | DIO17 | R/W | 0h | Data output enable for DIO 17 |
16 | DIO16 | R/W | 0h | Data output enable for DIO 16 |
15 | DIO15 | R/W | 0h | Data output enable for DIO 15 |
14 | DIO14 | R/W | 0h | Data output enable for DIO 14 |
13 | DIO13 | R/W | 0h | Data output enable for DIO 13 |
12 | DIO12 | R/W | 0h | Data output enable for DIO 12 |
11 | DIO11 | R/W | 0h | Data output enable for DIO 11 |
10 | DIO10 | R/W | 0h | Data output enable for DIO 10 |
9 | DIO9 | R/W | 0h | Data output enable for DIO 9 |
8 | DIO8 | R/W | 0h | Data output enable for DIO 8 |
7 | DIO7 | R/W | 0h | Data output enable for DIO 7 |
6 | DIO6 | R/W | 0h | Data output enable for DIO 6 |
5 | DIO5 | R/W | 0h | Data output enable for DIO 5 |
4 | DIO4 | R/W | 0h | Data output enable for DIO 4 |
3 | DIO3 | R/W | 0h | Data output enable for DIO 3 |
2 | DIO2 | R/W | 0h | Data output enable for DIO 2 |
1 | DIO1 | R/W | 0h | Data output enable for DIO 1 |
0 | DIO0 | R/W | 0h | Data output enable for DIO 0 |
EVFLAGS31_0 is shown in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_EVFLAGS31_0_FIGURE and described in #MCU_GPIO_MCU_GPIO_MAP1_MCU_GPIO_ALL_EVFLAGS31_0_TABLE.
Return to the Summary Table.
Event Register for DIO 0 to 31
Reading this registers will return 1 for triggered event and 0 for non-triggered events.
Writing a 1 to a bit field will clear the event.
The configuration of events is done inside MCU IOC, e.g. events for DIO #0 is configured in IOC:IOCFG0.EDGE_DET and IOC:IOCFG0.EDGE_IRQ_EN.
31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
DIO31 | DIO30 | DIO29 | DIO28 | DIO27 | DIO26 | DIO25 | DIO24 |
R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h |
23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
DIO23 | DIO22 | DIO21 | DIO20 | DIO19 | DIO18 | DIO17 | DIO16 |
R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h |
15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
DIO15 | DIO14 | DIO13 | DIO12 | DIO11 | DIO10 | DIO9 | DIO8 |
R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
DIO7 | DIO6 | DIO5 | DIO4 | DIO3 | DIO2 | DIO1 | DIO0 |
R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h | R/W1C-0h |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
31 | DIO31 | R/W1C | 0h | Event for DIO 31 |
30 | DIO30 | R/W1C | 0h | Event for DIO 30 |
29 | DIO29 | R/W1C | 0h | Event for DIO 29 |
28 | DIO28 | R/W1C | 0h | Event for DIO 28 |
27 | DIO27 | R/W1C | 0h | Event for DIO 27 |
26 | DIO26 | R/W1C | 0h | Event for DIO 26 |
25 | DIO25 | R/W1C | 0h | Event for DIO 25 |
24 | DIO24 | R/W1C | 0h | Event for DIO 24 |
23 | DIO23 | R/W1C | 0h | Event for DIO 23 |
22 | DIO22 | R/W1C | 0h | Event for DIO 22 |
21 | DIO21 | R/W1C | 0h | Event for DIO 21 |
20 | DIO20 | R/W1C | 0h | Event for DIO 20 |
19 | DIO19 | R/W1C | 0h | Event for DIO 19 |
18 | DIO18 | R/W1C | 0h | Event for DIO 18 |
17 | DIO17 | R/W1C | 0h | Event for DIO 17 |
16 | DIO16 | R/W1C | 0h | Event for DIO 16 |
15 | DIO15 | R/W1C | 0h | Event for DIO 15 |
14 | DIO14 | R/W1C | 0h | Event for DIO 14 |
13 | DIO13 | R/W1C | 0h | Event for DIO 13 |
12 | DIO12 | R/W1C | 0h | Event for DIO 12 |
11 | DIO11 | R/W1C | 0h | Event for DIO 11 |
10 | DIO10 | R/W1C | 0h | Event for DIO 10 |
9 | DIO9 | R/W1C | 0h | Event for DIO 9 |
8 | DIO8 | R/W1C | 0h | Event for DIO 8 |
7 | DIO7 | R/W1C | 0h | Event for DIO 7 |
6 | DIO6 | R/W1C | 0h | Event for DIO 6 |
5 | DIO5 | R/W1C | 0h | Event for DIO 5 |
4 | DIO4 | R/W1C | 0h | Event for DIO 4 |
3 | DIO3 | R/W1C | 0h | Event for DIO 3 |
2 | DIO2 | R/W1C | 0h | Event for DIO 2 |
1 | DIO1 | R/W1C | 0h | Event for DIO 1 |
0 | DIO0 | R/W1C | 0h | Event for DIO 0 |