SWRA446 February   2015 CC1310 , CC1310 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA

 

  1.   Using GCC/GDB With SimpleLink CC26xx/CC13xx
    1.     Trademarks
    2. 1 Introduction
    3. 2 Prerequisites
      1. 2.1 Platforms
      2. 2.2 Hardware
      3. 2.3 Software
    4. 3 Hardware Setup
    5. 4 Software Installation Instructions
      1. 4.1 Java Runtime Environment
      2. 4.2 Eclipse IDE (Windows)
      3. 4.3 Eclipse IDE (Linux)
      4. 4.4 GNU Toolchain (Windows)
      5. 4.5 GNU Toolchain (Linux)
      6. 4.6 Build Tools for Windows
      7. 4.7 TI Emupack and GDB Server (Windows)
      8. 4.8 Flash Programmer (Windows)
      9. 4.9 Flash Programmer (Linux)
    6. 5 Build the Software Example
      1. 5.1 Import Example Project Into the IDE
      2. 5.2 Build the Software Example
    7. 6 Load Binary Image to Target
      1. 6.1 Configure Flash Programmer Tool (Windows)
      2. 6.2 Configure Flash Programmer Tool (Linux)
      3. 6.3 Load the Image to Target (Windows)
      4. 6.4 Load the Image to Target (Linux)
    8. 7 Debug the Software Example
      1. 7.1 Launch the GDB Server (Windows)
      2. 7.2 Launch the GDB Server (Linux)
      3. 7.3 Configure Eclipse Debugger
      4. 7.4 Running the Software Example From Debugger
    9. 8 References
  2. AMakefile
    1. A.1 Makedefs
    2. A.2 Makefile
  3. BLinker and Startup Files
    1. B.1 Linker File
    2. B.2 Startup Files

GNU Toolchain (Windows)

GNU Tools for ARM Embedded Processors is a free package that includes the GNU compiler and linker tools as well as the GNU debugger. Perform the following steps for Windows installation:

  1. Download GNU Tools for ARM Embedded Processors. The package can be found on this site: https://launchpad.net/gcc-arm-embedded.
  2. Run the installer and follow the instructions. In the last step, make sure to select the checkbox 'Add path to environment variable'.
  3. Verify from the command prompt that the package is installed is updated correctly. This can be done by clicking Start → Run… . Type in cmd and click OK. In the command window, write:
  4. arm-none-eabi-gcc --version

    The expected output is shown in Figure 6. If the arm-none-eabi-gcc program is not found, check that the PATH variable is correctly set.

    sourcery_codebench_lite_windows_swra446.gifFigure 6. GNU Toolchain (Windows)

More information about this package can be found in [3].