This application report presents the concept of beacons by using Bluetooth low energy technology. The important parameters when designing beacon solutions are elaborated on a detailed level throughout the document. With the use of the TI Bluetooth low energy-Stack, beacons can be done in a simple and intuitive way.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
Wi-Fi is a registered trademark of Wi-Fi Alliance.
All other trademarks are the property of their respective owners.
A beacon in wireless technology is the concept of broadcasting small pieces of information. The information may be anything, ranging from ambient data (temperature, air pressure, humidity, and so forth) to micro-location data (asset tracking, retail, and so forth) or orientation data (acceleration, rotation, and so forth).
The transmitted data is typically static but can also be dynamic and change over time. With the use of Bluetooth low energy, beacons can be designed to run for years on a single coin cell battery. This application report introduces the concept of beacons and how to get started with implementing a beacon solution. Naming conventions throughout this document can be summarized as Beacons that broadcast information by using advertisements with Bluetooth low energy technology that could be branded as Bluetooth low energy.
A Bluetooth low energy device can operate in four different device roles. Depending on the role, the devices behave differently. The first two roles are connection-based:
This means that the device roles used for established connections are the Peripheral and the Central roles. The other two device roles are used for one-directional communication:
The two obvious device roles for beacon applications are Peripheral and Broadcaster. Both of them send the same type of advertisements with the exception of one specific flag that indicates if it is connectable or non-connectable. A Peripheral device that implements a GATT Server (GATT is an architecture for how data is stored and exchanged between two or more devices) can be branded as a Bluetooth low energy device. So a Bluetooth low energy branding indicates that the device is a connectable Peripheral device that has data, which could be interacted with.
A Bluetooth low energy solution is ideal for beacons because it is low power and the eco-system is already deployed in the majority of smartphones or other Bluetooth low energy enabled devices on the market. The low-power consumption is achieved by keeping the transmission time as short as possible and allowing the device to go into sleep mode between the transmissions.