SWRA495K December 2015 – April 2024 CC1310 , CC1350 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R-Q1 , CC2650 , CC2662R-Q1
A crystal has two resonant frequencies characterized by a zero-phase shift. Equation 1 is the series resonance.
Equation 2 is the anti-resonant frequency.
As specified in the data sheet of the crystal, the frequency of oscillation is between the resonance frequencies. See Equation 3.