SWRA536 February 2016 CC2520 , CC2520 , CC2530 , CC2530 , CC2530-RF4CE , CC2530-RF4CE , CC2533 , CC2533 , CC2540 , CC2540 , CC2541 , CC2541 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2640R2L , CC2640R2L , CC2650 , CC2650 , CC2650MODA , CC2650MODA
Level | PEP | Ok Pkt | PER[%] |
---|---|---|---|
-105.0 | -82.29 | 148 | 1.33 % |
-106.0 | -83.29 | 141 | 6.00 % |
-107.0 | -84.29 | 132 | 12.00 % |
-108.0 | -85.29 | 117 | 22.00 % |
-108.6 | -85.89 | 104 | 30.67 % |
-109.0 | -86.29 | 94 | 37.33 % |
-110.0 | -87.29 | 45 | 70.00 % |
Measured sensitivity at 2480 MHz was found to be -85.89 dBm PEP. The wanted signal should, according to the Receiver Blocking Parameters Receiver Category 2 Equipment table in ETSI EN 300 328 V2.1.1, be set 6 dB above the sensitivity limits. With a measured sensitivity of -85.89 dBm this leads to that the level on the wanted signal being -79.89 dBm PEP (level = -102.2 dBm).
Note that there is a loss in the test setup of almost 10 dB (see Section 4.1) so actual sensitivity level is around -96 dBm.