SWRA536 February 2016 CC2520 , CC2520 , CC2530 , CC2530 , CC2530-RF4CE , CC2530-RF4CE , CC2533 , CC2533 , CC2540 , CC2540 , CC2541 , CC2541 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2640R2L , CC2640R2L , CC2650 , CC2650 , CC2650MODA , CC2650MODA
Loss for the TX CW blocker through cables, splitter and coupler from the signal generator in the test setup needs to be measured and compensated to get the correct measurement results.
The cable connected to the DUT is connected to the spectrum analyzer and the power level of the TX CW is measured at the different TX CW test frequencies. The difference between the TX CW source output power and the power applied to the DUT is calculated and used to compensate the measurement result presented in Section 4.4.
2380.0 MHz | 2503.5 MHz | 2300.0 MHz | 2583.5 MHz | |
---|---|---|---|---|
Blocker output [dBm] | -30.0 | -30.0 | -30.0 | -30.0 |
@ Coupler [dBm] | -47.8 | -47.2 | -47.5 | -48.1 |
@ DUT [dBm] | -39.9 | -39.8 | -39.8 | -40.5 |
Loss in test setup [dB] | -9.9 | -9.8 | -9.8 | -10.5 |