SimpleLink and SmartRF are trademarks of Texas Instruments Incorporated.
Zigbee is a registered trademark of ZigBee Alliance.
Wi-SUN is a registered trademark of Wi-SUN Alliance.
Bluetooth is a registered trademark of Bluetooth SIG, Inc.
All trademarks are the property of their respective owners.
The SimpleLink CC1352P and CC2652P devices are multiprotocol, multi-band, Sub-1 GHz and 2.4 GHz wireless MCUs supporting Wireless M-Bus, IEEE 802.15.4g, IPv6-enabled smart objects (6LoWPAN), Thread, Zigbee®, KNX RF, Wi-SUN®, Bluetooth® 5 Low Energy, and proprietary systems. The devices contain an integrated high-power amplifier (PA) with best-in-class efficiency for long-range applications delivering up to 20 dBm.
The current consumption for 20 dBm output power at 2.4 GHz is more than 80 mA, and not suitable for applications running off of small size batteries such as coin cells. To mitigate this constraint, this application report documents how the PA can be optimized to achieve its highest efficiency at 10 dBm output power, reducing the peak current consumption to only 22 mA at 3.0 V. 10 dBm output power is selected because for several popular protocols, it is the highest allowable power level in Europe.
Two things are required to optimize the PA for 10 dBm operation: a dedicated RF matching network and dedicated radio configuration settings. The former is covered in this document, while the latter is found in the applicable SDKs and SmartRF™ Studio software.
The RF matching network consists of a balun and filter. The combination of the balun and filter also transforms the complex differential output impedance of the PA to 50 Ω. Furthermore, the PA is biased (powered) through the external RF network. To output 20 dBm, the PA is biased from VDDS to allow a large enough voltage swing.
To optimize the PA for 10 dBm operation, two changes must be done:
The resulting recommended schematic for 10 dBm PA operation is shown in Section A.1.
For this design, external load capacitors for the 48 MHz crystal should be used to reduce clock spurs.
The layout is based on the CC1352PEM-XD7793-XD24-PA24 design files. The top layer is equal to the top layer from the RF pins to the 50 Ω point, except for the biasing the RF network from VDDR instead of VDDS.
The EVM used for the test results presented in this application report, as well as in the CC1352P SimpleLink™ High-Performance Dual-Band Wireless MCU With Integrated Power Amplifier Data Sheet or the CC2652P SimpleLink™ Multiprotocol 2.4 GHz Wireless MCU With Integrated Power Amplifier Data Sheet (SWRS195), connects the PA output directly to an SMA connector. In a typical application, you would use an RF switch to combine the PA output with the regular 2.4 GHz RF matching for Rx. For an application example, see the LAUNCHXL-CC1352P-2 Design Files. To account for the typical loss in such an RF switch, the 10 dBm output power setting is tuned to output 10.5 dBm on the test EVM.
According to EN300 328 max output power is 10 dBm/MHz E.I.R.P. Depending on the data rate and antenna gain, this may limit the maximum conducted output power delivered to the antenna.
To ensure margins for passing FCC band edge requirements at 2480 MHz for Zigbee, back-off of the output power has to be evaluated.
For performance data, see the CC1352P SimpleLink™ High-Performance Dual-Band Wireless MCU With Integrated Power Amplifier Data Sheet or the CC2652P SimpleLink™ Multiprotocol 2.4 GHz Wireless MCU With Integrated Power Amplifier Data Sheet.
For some units, the conducted output power will be higher than the ETSI and FCC limit for frequencies ranging between 200 MHz to 300 MHz. Energy in this frequency range will be attenuated by the antenna and radiated measurements will pass.
The following is valid for SmartRF Studio 2.19 or later.
To export the settings required, do the following in SmartRF Studio:
The settings are characterized for BLE and Zigbee but may be used for proprietary.