The following is valid for SmartRF
Studio 2.19 or later.
To export the settings required, do
the following in SmartRF Studio:
- Open CC1352P. Select either "BLE
mode" or "IEEE 802.15.4 mode"
- In the "RF Design Based On"
pulldown, select "LAUNCHXL-CC1352P-4"
The settings are characterized for BLE
and Zigbee but may be used for proprietary.
WARNING: The settings can
only be used with hardware where the high-power PA is biased from VDDR. If the
high-power PA is biased from VDDS, and these settings are used, the PA will operate
outside the recommended operating conditions.