SWRA657 June 2020 CC3100 , CC3200
All systems using serial flash are vulnerable to the effects of sudden power removal. As noted in most serial flash data sheets, data corruption may occur if the power is removed while a write/erase operation is in progress. This can happen if the system operating voltage goes below Vmin of the serial flash (2.3 V typical) before the erase/write operation is completed. Figure 5 shows a typical scenario.
This scenario may occur in battery or line powered end equipment.
The sections below explain how the potential for serial flash corruption can be minimized in both types of end equipment.