SWRA682 December 2020 CC1310 , CC1312PSIP , CC1312R , CC1314R10 , CC1350 , CC1352P , CC1352P7 , CC1352R
The anti-aliasing BW (AABW) should be as low as possible to give best possible blocking. The AABW is set by the following override:
ADI_HALFREG_OVERRIDE(0,61,0xMask,0xValue). Mask is a bit mask. This is typically set to 0xF. "Value" is 4 bits where a lower value gives larger bandwidth.
Find the anti-aliasing bandwidth that gives a marginal decrease in sensitivity and select a setting value that is two settings below this. Meaning if tests using 0x09 starts to give a reduced sensitivity, 0x07 should be used.