SWRA754 april 2023 AWRL6432 , IWRL6432
The IWRL6432BOOST EVM allows users to measure the power consumed by the xWRL6432 device through the INA current sense amplifiers onboard. The motion and presence detection demo provided in the xWRL6432 SDK includes an output that shows the average current measured on the power rails provided to the device. Additionally, the I2C interface that reads from the INA current sense amplifiers can also be read from an external microcontroller for situations where recording the output on the xWRL6432 device is not feasible (e.g. measuring deep sleep power). See [2] for details on how to enable and interpret the power measurement packets.
The Rev A. and Rev B. IWRL6432BOOST do not provide the ability to measure power accurately due to the limitations of the INA226 devices placed onboard. The Rev A. and Rev B. IWRL6432BOOSTs require the following changes to measure power properly.
Reference Designator |
Initial Device |
Replacement Device |
---|---|---|
R200, R192, R193 |
PMR18EZPFV2L00 2 mΩ Resistor |
WSL1206R0400FEB 40mΩ Resistor |
R134 |
PMR18EZPFV2L00 2 mΩ Resistor |
WSL1206R0200FEB 20mΩ Resistor |
U6, U7, U8, U25 |
INA226AIDGST Current Monitor |
INA228AIDGST Current Monitor |