SWRA769 august 2023 CC2564C
This section provides a description of how to use the demo application to connect two configured boards and communicate over Bluetooth®. The Bluetooth HFP is a simple client-server connection process with one side operating in the Audio-Gateway role and the other operating in the Hands-free role. Set-up one of the boards as an Audio-Gateway client (HFPAGDemo acts as Audio gateway) and set-up another board as a hands-free server (using HFP Demo). This will initiate a connection and send indications between the two devices over Bluetooth. Now use the second board and follow the steps as per either HFP Demo when using Tiva or MSP430 as the server or HFPDemo_HF for MSP432or STM32F4 as the server. Perform the steps prior to running the Audio-Gateway Bluetooth code on the first board. The second device that is connected to the computer will be the hands-free server.