SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Set Speaker Gain

Description

The following function is responsible for setting the Speaker Gain on Remote Device. This function returns zero on successful execution and a negative value on all errors. This function works if the remote audio volume control feature is supported in the HF device.

Parameters

The command only requires an integer value for the Speaker Gain as a parameter.

Command Call Examples

  • "SetSpeakerGain 5"
  • "SetSpeakerGain 6"

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Set_Remote_Speaker_Gain(BluetoothStackID, CurrentClientPortID, TempParam->Params->intParam)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Set_Remote_Speaker_Gain(unsigned int BluetoothStackID, unsigned int HFREPortID, unsigned int SpeakerGain)

Description of API

This function is responsible for allowing synchronization and setting of the Remote Devices Speaker Gain. This function can only be performed if a valid Service Level Connection exists. When called by a Hands-Free unit this function is provided as a means to inform the Remote Audio Gateway of the current Speaker Gain value. When called by an Audio Gateway this function provides a means for the Audio Gateway to control the Speaker Gain of the Remote Hands-Free unit. This function accepts as its input parameters the Bluetooth Stack ID for which the HFRE Port ID is valid as well as the HFRE Port ID. The final parameter is the Speaker Gain to be sent to the Remote Device. The Speaker Gain Parameter *MUST* be between the values of HFRE_SPEAKER_GAIN_MINIMUM and HFRE_SPEAKER_GAIN_MAXIMUM. This function returns zero if successful or a negative return error code if there was an error.