SWRA772 august 2023 CC2564C
The Help command is responsible for displaying the current Command Options for either Serial Port Client or Serial Port Server. The input parameter to this command is completely ignored, and only needs to be passed in because all Commands that can be entered at the prompt pass in the parsed information. This command displays the current command options that are available and always returns zero.
Including parameters is not necessary when using this command. A parameter has no effect on the outcome of the command.
This command always returns 0.