SWRA824 October 2024 CC1120
The test platform included the conducted emissions test board powered by a 24V DC input. This board was then connected to the Smart RF transceiver evaluation board, used in combination with Smart RF Studio, which allows for user access to the devices registers for configuration of the radio parameters and behavior. It also provides a control interface for performing operations such as setting up a continuous wave signal, which was used in this application. Lastly, a spectrum analyzer was connected to the radiated emissions test board to measure the frequency response at the antenna.
Figure 5-1 shows the setup used for testing.
Each buck converter was tested at a transmission power of 0dBm and 15dBm. The span was set to 500kHz and the resolution and video bandwidth were set to 4.7kHz. The following spectrums were observed.
The LMR36510 and LMR36506 were then tested at an increased span to identify any potential spurs outside of the original 500 kHz span.
After observing that the LMR36506 and LMR36510 exhibit improved harmonic distortion compared to the control unit, additional testing was conducted by adjusting the switching frequency of the LMR36506 to determine if further improvements were possible.
Based on the frequency spectrums above, the LMR36510 was seen to have the best performance with respect to reducing spurious emissions as shown in Figure 5-10 and Figure 5-8.