SWRU271I October 2010 – January 2020 CC2540 , CC2540T , CC2541 , CC2541-Q1 , CC2640R2F
This section describes the vendor specific HCI Extension API. These proprietary commands are specific to the CC254x device. Where more detail is required, an example is provided.
NOTE
Unless stated otherwise, the return values for these commands is SUCCESS. This value does not indicate successful completion of the command. These commands result in corresponding events that you should check by the calling application