This document is a guide through the initial steps required to run the preprogrammed Bluetooth® low energy (BLE) Keyfob demo application.
SimpleLink is a trademark of Texas Instruments.
Bluetooth is a registered trademark of Bluetooth SIG Inc..
iOS is a trademark of Cisco.
Windows is a registered trademark of Microsoft Corp..
The RF boards in this kit are designed to comply with ETIS, FCC, and IC regulations over a temperature from 0°C to +35°C. The kit is for evaluation only; it is not FCC approved for resale.
CAUTION
The kit contains ESD sensitive components. Handle with care to prevent permanent damage.