SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The SimpleLink Wi-Fi device provides comprehensive networking functionality. To simplify the integration and development of networking applications, a simpler, user-friendly host driver is provided. The SimpleLink Wi-Fi host driver is responsible for the following:
The SimpleLink Wi-Fi host driver is written in strict ANSI C89 for full compatibility with most embedded platforms and development environments.
The following information is relevant for the SimpleLink Wi-Fi CC31xx wireless network processor, which must implement a communication interface with a selected MCU.
The device supports the SPI and UART standard communication interfaces. Binding the communication interface to the host driver is done by defining the interface functions through the following defines in user.h: