SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The SimpleLink device supports Wi-Fi enterprise connection, according to the 802.1x authentication process. An enterprise connection requires the radio server behind the AP to authenticate the station. The following authentication methods are supported on the device:
After the station has been authenticated, the AP and the station negotiate WPA(1/2) security.