SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
P2P configuration uses the host driver APIs that control the simplelink WiFi device. Different options and modes of P2P configuration can be accessed by using specific APIs. By using a specific APIs, the user can set P2P abilities and use them. The configuration is divided to few easy sections. The configuration of specific sections has an influence on the configuration of others sections.
The configuration is divided into these sections:
The next section explains how to configure P2P and how to use its options. Note that: