SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
The Rx-filters module lets the user define a set of rules that will determine which of the received frames will be transferred by the SimpleLink WiFi device to the host, and which frames will be dropped. The Rx-filters can be activated during AP-connection and during promiscuous mode (“disconnect mode”).