6.1 Visual Studio Installation
Download and install Visual Studio. In this tutorial, we are using the Visual Studio 2015 Community Edition.
- Run the installer to install Visual Studio. On the Customization page, select Custom. On the Select Features page, ensure the Visual C++ option under Programming Languages is checked, as shown in Figure 33.
NOTE
Installation may take a while to complete, depending on the number of selections and network speed, because Visual Studio must download these files.
- Once installation is complete, restart Visual Studio by clicking the Restart button.
- After restarting, a dialog box requiring an update to additional packages may appear, as shown in Figure 34. Click Next and then Update.