SWRU523C June 2020 – May 2022 CC2560 , CC2564 , CC2564C , CC2564MODA , CC2564MODN
Texas Instruments™, MSP430™, CapTIvate™, LaunchPad™, SimpleLink™, MSP432™, Sitara™, Tiva™, and BoosterPack™ are trademarks of Texas Instruments.
Amkor Technology™ is a trademark of Amkor Technology.
Bluetooth® is a registered trademark of Bluetooth SIG, Inc.
Arm® and Cortex® are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
Linux® is a registered trademark of Linus Torvalds in the U.S. and other countries.
STM32® is a registered trademark of STMicroelectronics International N.V.
Wi-Fi® is a registered trademark of Wi-Fi Aliance.
iPod® and Apple® are registered trademarks of Apple Inc.
Bluetopia® is a registered trademark of Stonestreet One, LLC.
All trademarks are the property of their respective owners.
Table 1-1 lists the device and module options.
Property | Devices and Modules | ||||
---|---|---|---|---|---|
![]() |
![]() |
![]() |
![]() |
![]() |
|
CC2564C | CC2564MODA | CC2564MODN | CC2564 | CC2560 | |
Bluetooth BR-EDR | √ | √ | √ | √ | √ |
Bluetooth Low Energy | √ | √ | √ | √ | — |
Module or IC | IC | Module | Module | IC | IC |
FCC, IC, CE certification | — | √ | √ | — | — |
Bluetooth certification | 5.1 (compliant) | 4.1 | 4.1 | 4.1 | 4.1 |
Internal antenna | — | √ | — | — | — |
For more information about the CC256x devices, see the CC256x wiki page.
Ask questions and solve problems with fellow engineers on our E2E Dual-Mode Bluetooth® Forum.
The following blog is applicable to the devices in the CC256x family:
Three reasons why our dual-mode Bluetooth stack is your new go-to software solution