SWRU529C May 2017 – April 2020
If users want to save the incoming processed stream from the mmWave device for some offline analysis while its getting plotted, they can use the Record Start button in the plots tab. The recording can be started while the device is in stopped state and unconfigured (for example, after a fresh reboot and/or the sensor is stopped using the Sensor Stop button), or while the device is running and actively outputting data. The data is saved to a timestamped file in binary format on the device. The data keeps accumulating in the file until one of the following conditions are met:
The data saved in this file is the exact same data and format that is transmitted out of the mmWave device over the DATA_port. Users should see the mmWave demo doxygen in the mmWave SDK package to understand the format of the data and how to parse it.
NOTE
This feature requires the browser version to be at least as mentioned here:
ti-widget-streamsaver.