SWRU529C May 2017 – April 2020
This is a slider that prompts users to select the desired Maximum Unambiguous Range in steps of 5 meters. Select the value based on the farthest distance you expect to see objects detected. See Section 4.3 to understand the radar cross section and the actual range at which objects equal to the radar cross section can be theoretically detected by mmWave technology.
Effects on other user knobs:
CLI command details: defines the frequency slope constant in the profileCfg command.