SWRU587A November 2021 – March 2023 AWR2944
The following are some guidelines for selecting the plots and frame rate:
User should select the following baud rates for DATA_port in the "Serial port" dialog using custom values when using mmW demo from mmWave_mcuplus_SDK as For SDK version <= 4.3, use 852272 for AWR294X and 892857 for AM273X. For SDK version >= 4.4, use 3125000 for both AWR294X and AM273X.