SWRU620A April 2024 – December 2024
J5 provides access to the onboard XDS110 (TM4C1294NCPDT) emulator. This connection provides the following interfaces to the PC:
When used in standalone mode of operation as shown in Figure 2-25, the power is supplied through a single USB connector; the same USB connector J5 is also used for configuration and data transfer through the XDS110 USB to UART converter. When enumerated correctly, the 2 UART ports from the XDS110 are displayed on the device manager as a virtual COM Port, similar to that shown in Figure 2-24.
If the PC is unable to recognize the above COM ports, Then install the latest EMUpack. Similar to that shown in Figure 2-23.
EVM uses single UART port for both device configuration and processed data communication to PC.