Press the Reset switch (Section 2.2.2) to make sure that the board boots up in the right mode.
Run the mmWave Visualizer inside
mmWave-L-SDK tool folder and use the flashing tab and follow the instruction or
use Uniflash tool. Similar to that shown in Figure 3-1.
Enter the application port number
for the flashing interface.
Select the image to flash to the
EVM in the Image Flash menu, or directly upload the image from the mmWave
SDK
(C:\ti\MMWAVE_L_SDK\examples\mmw_demo\motion_and_presence_detection\prebuilt_binaries\xwrL64xx).
Load appimage to serial flash. Similar to that shown in Figure 3-2. Please
refer mmWave SDK for the flash binary for running out of box demos.