The IWRL6432AOPEVM includes three
receiver and two transmitter short range antennas on the package of the chip.Figure 1-3 shows the antenna on package.
Note: There should not be any taller components in the Field Of
View (FOV) of the antenna to avoid any multipath reflection. We should also have a
keep out area of at least one wavelength (5mm) from either edge of the
device.
Figure 1-3 AOP Antennas
Figure 1-4 IWRL6432AOP Antenna Placement
MIMO Array