SWRU624A April   2024  – July 2024 CC3301 , CC3301MOD

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Download Prerequisites
  5. 2Build Prequisites
  6. 3Patch Steps
    1. 3.1 Additional Steps
    2. 3.2 Overall Steps
  7. 4Check the Applied Patch
  8. 5Build Steps
  9. 6Using the Built App File
  10. 7Revision History

Download Prerequisites

The QuickTrack Control App is a Wi-Fi automation test tool utilized for Wi-Fi Certification. This user guide is intended to provide an overview of using the QuickTrack Control App with the CC33xx devices to certify end products. The required software and set-up steps vary slightly between Linux® and Windows® operating software.

Note that Git Bash for Windows must be downloaded when using a Windows operating system.

The source files required to build and use the QuickTrack Control App can be cloned or downloaded and extracted from GitHub. It is imperative that the tags and checkouts are verified to ensure that the correct version is downloaded.

After using one of the above options to acquire the source file, the installer specific to the operating system being used must be downloaded. Both installers can be found on ti.com at the link below. Make sure to involve the appropriate installer file that corresponds to the operating system being used (Windows or Linux).