SWRU629 September 2024
The CC35xxE includes two independent UART peripherals, UART0 and UART1. The LP-EM-CC35X1 allows you to interface to these UART signals via the LaunchPad header pins.
UART1 interface is by default connected to the 20-pin LP-XDS110 header (J7) for serial terminal interface (COM port) to a PC via the LP-XDS110. For more information on this header, see Section 2.1.1.
The routing selection of the UART1 TX and RX signals to header J7 or to the LaunchPad header pins is performed using onboard jumpers, J4 and J6, as seen in the figures below.