SWRU629 September 2024
To enable the CC35xxE device, the nRESET line must be pulled high externally. On the LP-EM-CC35X1, the nRESET line is pulled up by default, therefore, the CC35xxE device is enabled when power is provided to the board.
The LP-EM-CC35X1 gives the option to route the Reset line to the LaunchPad header (pin 16) to control the reset line externally. To route the nRESET line to the LaunchPad header pin instead of the default pull up, jumper J9 needs to be placed on the bottom two pins. J9 is in the pull up (PU) configuration, therefore, the nRESET line is pulled up when power is supplied to the board, as shown in.Figure 2-15