The AWR2E44PEVM can be connected to the DCA1000 EVM platform to allow for LVDS data streaming. Figure 2-19 shows the AWR2E44PEVM interfaced to the DCA1000 EVM.
When using the AWR2E44PEVM with the DCA1000 EVM and mmWave Studio, the following settings must be used.
- Set the AWR2E44PEVM to SOP2 mode.
Set the AWR2E44PEVM switch S2 to FTDI_SPI Mode
- Set the DCA1000 EVM switches to the following configuration.
- The 5-V/12-V supply must be connected to J12 on the AWR2E44PEVM
- A 5-V supply must be connected to J2 on the
DCA1000 EVM (Do Not Exceed 5-V)
- A micro USB cable must be connected to the FTDI port on the AWR2E44PEVM (J10)
- The Samtec ribbon cable must be connected to J7 on the AWR2E44PEVM and J3 on the DCA1000 EVM
- An RJ45 cable must be connected to J6 on the DCA1000 EVM