SWRZ062F September 2015 – December 2022 CC1310
Motorola® SPI Format Slave Mode Writes to Transmit FIFO Can Lose Data
A and B
If the SSI is configured to operate in Motorola® SPI format slave mode, loss of write data can occur when the following two conditions are met:
For more details, see the Synchronous Serial Interface (SSI) chapter in the CC13x0, CC26x0 SimpleLink™ Wireless MCU Technical Reference Manual.