SWRZ102C November 2021 – December 2024 AWR2944
PRODUCTION DATA
Second Harmonic (HD2) Present in the Receiver
AWR294x ES2.0
There is a finite isolation between the RF pins/package and the FMCW synthesizer. This can create spurious tones at the synthesizer output and lead to appearance of 2nd order harmonics and inter-modulations of expected IF frequencies at RX ADC output. The amplitude of the 2nd harmonic could be as high as -30 dBc , referenced to the power level of the intended tone at the LNA input.
No workaround available at this time. However, in many typical radar use cases the HD2 does not affect the system performance due to two reasons: