SWRZ102C November 2021 – December 2024 AWR2944
PRODUCTION DATA
HPF cutoff frequency 2800kHz configuration can result in incorrect RX IFA gains and filter corner frequencies.
AWR294x ES2.0
The analog IF stages include a second order high pass filter that can be configured to the following -6dB corner frequencies :
300, 350, 700, 1400, 2800 KHz.
Out of these, HPF cutoff frequency 2800kHz configuration can result in incorrect RX IFA gains and filter corner frequencies.
Use of 2800kHz cutoff configuration is not recommended.