SWRZ116 February 2022 CC2652RSIP
PRODUCTION DATA
Arm® Errata #752770: Interrupted Loads to SP Can Cause Erroneous Behavior
Revision F
An interrupt occurring during the data-phase of a single word load to the stack-pointer (SP/R13) can cause an erroneous behavior of the device. In all cases, returning from the interrupt will result in the load instruction being executed an additional time. For all instructions performing an update to the base register, the base register will be erroneously updated on each execution, resulting in the stack-pointer being loaded from an incorrect memory location.
The affected instructions that can result in the load transaction being repeated are:
The affected instructions that can result in the stack-pointer being loaded from an incorrect memory address are:
Conditions:
Implications:
Unless the load is being performed to device memory or strongly-ordered memory, there should be no implications from the repetition of the load.
Most compilers ensure this bug is not triggered by not emitting the affected instruction sequence and not using the instructions in the compiler runtime libraries. This includes:
A workaround for both issues can be implemented by replacing the direct load to the stack-pointer, with an intermediate load to a general-purpose register followed by a move to the stack-pointer.
If repeated reads are acceptable, then the base register update issue may be worked around by performing the stack-pointer load without the base increment followed by a subsequent ADD or SUB instruction to perform the appropriate update to the base register.