TIDT205 February 2021
Efficiency was taken with the converter operating with 13.5-V input, 5-V output. The input supply was connected directly at the input of the converter. All other converters on the board were disabled. Peak efficiency is over 91%.
Efficiency was taken with the converter operating with 5-V input, 3.3-V output. The input supply was connected directly at the input of the converter. All other converters on the board were disabled. Peak efficiency is over 90%.
Efficiency was taken with the converter operating with 5-V input, 1.8-V output. The input supply was connected directly at the input of the converter. All other converters on the board were disabled. Peak efficiency is over 89%.
Efficiency was taken with the converter operating with 5-V input, 1.35-V output. The input supply was connected directly at the input of the converter. All other converters on the board were disabled. Peak efficiency is over 88%.
Efficiency was taken with the converter operating with 5-V input, 1.175-V output. The input supply was connected directly at the input of the converter. All other converters on the board were disabled. Peak efficiency is over 86%.