TIDT321 January 2023
Load transient response is shown in the following figures.
The waveform in Figure 3-5 was created using the following conditions: input voltage = 565 VDC; load
transient = 200 mA to 1 A.
The waveform in Figure 3-6 was created using the following conditions: input voltage = 565 VDC; load
transient = 500 mA to 1 A.