TIDUAH1A August   2015  – April 2018

 

  1.   Revision History

Connectors

Table 10. Connector Details

INPUT/OUTPUT TYPE SPECIFICATION CONNECTOR
INPUTS
Voltage I/P Channel 1 J11
Channel 2 J12
Channel 3 J13
OUTPUTS
Analog Output Analog Output 0 (AOUT0) J9.3 – J9.4
Analog Output 1 (AOUT1) J9.1 – J9.2
Analog output parameter selection(1)
(connect jumper between mentioned pins)
Phase 1 (AOUT0 = V1; AOUT1 = I1) J4.1 – J4.2
Phase 2 (AOUT0 = V2; AOUT1 = I2) J4.3 – J4.4
Phase 3 (AOUT0 = V3; AOUT1 = I3) J4.5 – J4.6
Analog output type (voltage ±10 V or current ±24 mA) selection
(connect jumper between mentioned pins)
AOUT0 = ±10-V voltage mode J3.2 – J3.3
AOUT0 = ±24-mA current mode J4.7 – J4.8,
J3.2 – J3.3
AOUT1 = ±24-mA current mode J3.2 – J3.3
AOUT1 = ±10-V voltage mode J4.9 – J4.10,
J3.2 – J3.3
Digital (relay) output (connect 8.5 V or higher on J1.2 to J2.1 for operation of relay driver IC) Channel 1 J1.8 – J1.1
Channel 2 J1.7 – J1.1
Channel 3 J1.6 – J1.1
Channel 4 J1.5 – J1.1
Channel 5 J1.4 – J1.1
Channel 6 J1.3 – J1.1
POWER SUPPLY
Non-isolated power supply input 12-V dc J8.1 wrt J8.2
Isolated power supply input 15-V dc J14.1 wrt J14.4
–15-V dc J14.2 wrt J14.4
MCU
MCU programming JTAG J10
Expansion I/O interface SPI, I2C, UART, and GPIO J5, J2, J4
Analog output parameter selection: The appropriate phase jumper must be connected. The analog output is at mid-value and no data sends in the case that no jumper is connected for the phase selection. In the case where multiple jumpers are connected for phase selection, priority is given as per phase 1 > phase 2 > phase 3. For example, if phase 1 and phase 2 jumpers are connected, phase 1 receives priority and phase 1 data sends to the analog outputs.

The current input wires are taken through the current transformer and do not have connectors (see Figure 22). The wires are connected externally as flying leads. An external terminal block can be used to connect the current inputs.

TIDA-00454 Current_Input_Wire_TIDUAH1.gifFigure 22. Current Input Wire Through CT

Figure 23 shows the interface connectors for the TIDA-00454 board.

TIDA-00454 TIDA-00454_Interface_Connectors_TIDUAH1.gifFigure 23. TIDA-00454 Interface Connectors